Other Parts Discussed in Thread: Z-STACK, SIMPLELINK-CC13XX-CC26XX-SDK
Hi, i hope this doesn't sound too stupid. I want to practice zigbee development and find a way to add a set of devices into groups of varying size at runtime from a coordinator device. I imagine this is similar to the way home automation apps work where you can create groups of devices from their web application.
However, there's a few thing which are unclear to me:
- How can i know which device is which? If i have tens of devices, that means i have to hold a container of tens of short addresses inside my coordinator, so i can always associate device X with its address?
- All i have to do is send the "Add Group" command from the coordinator to the desired device?