This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531: How to connect end device

Part Number: CC2531

Hi all,

I followed this example: https://sunmaysky.blogspot.com/2017/02/use-ztool-z-stack-30-znp-to-set-up.html and have successfully made one of my CC2531 a Coordinator and another CC2531 a router.
I then unplug the Coordinator and use the CC debugger to flash a Wireshark Zigbee Packet Sniffing hex file into it and it is able to sniff IEEE802.15.4 as well as Zigbee packets. However, I have been using Z-tool 2.0 with the Router CC2531 to do some configurations to allow my XB3-24Z8UM (A Zigbee chip) to join the network and it is to no avail.
Configurations were done through Z-tool 2.0 with commands like ZDO_MGMT_PERMIT_JOIN_REQ
ZB_FIND_DEVICE_REQ and ZB_PERMIT_JOINING_REQ

I am able to receive Beacon Requests and a Beacon is being sent from the Router CC2531, yet I am unable to connect my XB3-24Z8UM to the Zigbee Network.
Any advice?

Best Regards,
Marcus