Other Parts Discussed in Thread: CC1352R,
Hello,
We are looking into using an SOC in the CC1352 line for dual band operation. The Sub-GHz will be used for our proprietary controls, but we are looking into offering several protocol options for the 2.4 GHz band. I noticed that only the datasheet for CC1352P7 lists Matter as an included protocol, but the Matter github lists CC1352R as a build option with limited capabilities. To run a full Thread device with BLE, will the extra flash for the CC1352P7 be required? If we are planning to add Matter as a protocol, will we need an external flash chip for performing OTA updates (either due to flash requirements or ability to update the additional ROM on the chip)?
Thanks