This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZStack-EXP5438-2.4.0-1.4.0



Hi,

I am using IAR EW  for MSP430 ver 5.20 to compile and run ZStack-EXP5438-2.4.0-1.4.0. When I try to download and debug the program, it gives the following error message:
The debugging session could not be started.
Either the debugger initialization failed, or else the file "<Project path\project_name>.d43" was corrupt or of an unsupported format.

The hardware I am using is TI's MSP-EXP430F5438 Development boards and MSP430 USB-Debug-Interface -- MSP-FETU430IF debugger.

Kindly suggest how to fix this issue.

Best regards,
Hariprakash.