This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: How to configure attribute reporting on CC1352P with Z-stack

Part Number: CC1352P

Hi,

SDK:   simplelink_cc13x2_26x2_sdk_5_20_00_52

Demo: zc_doorlockcontroller + zr_doorlock

    In the demos, if the PINcode entered by the door lock controller is wrong, the door lock will report ZCL_STATUS_INVALID_VALUE to the controller indicates that the PIN code is incorrect.

    Now I want to add a function on this basis: after reporting the ZCL_STATUS_INVALID_VALUE, report a prompt string, such as "PIN code starts from 1".

    I am not familiar with the attribute reporting configuration and reporting implementation process. Is there any method to realize this function?

Please help, thank you!

BR,

Siemin