Other Parts Discussed in Thread: CC2538, Z-STACK
Dear all,
I learnt the secure rejoin and insecure rejoin in the link (https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/701530/cc2538-rejoin-policy-in-zigbee-3-0-1 ).
If I want to test the insecure rejoin in two CC2538 boards, I need to change
(1) the controller setting (removing device validation from ZDSecMgrDeviceJoin)
(2) the end device setting (Z-Stack currently processes rejoins as such: 1. Secure 1 channel 2.Secure all channels 3. Unsecure 1 channel 4. Unsecure all channels continuously.)
Right?
The question now is that I cannot find the settings of the end device, can I modify this part manually? If so, where is the settings? somewhere in bdb.c or other files?
Best Regards