Part Number: CC2652R
Other Parts Discussed in Thread: UNIFLASH,
Hello,
In the past I always used the XDS110 for debugging of our SimpleLink based products. It happened very often in the last weeks that it was not possible to start a debug session because the XDS failed with the following message:
Error initializing emulator: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 9.6.0.00172)
Today it reached a point where I can say that it is not usable anymore because it doesn't work to connect to a target or if it randomly does it will break up during the debug session. I downloaded the last CCS (11.1) because I thought that possible bugs will be solved in this version. Unfortunately it still doesn't work. After a restart it almost always work to connect to the target but if I stop the debug session and start it again it doesn't work.
I also checked it with the xdsdfu utility and if it is in this state where I cannot debug it also shows 0 devices in this tool. If I reconnect the device it shows up in xdsdfu.exe -e normally.
Flashing using Flash Programmer 2 also works without any problem. Uniflash doesn't always work perfectly.
Can you help me with this issue?
Thanks
Armin