Hello all,
I'm using Z-Tool for setting up a Zigbee network. I want to know that if there exists any command in Z-Tool that can send a direct join request to a device(not already a part of the network) from my coordinator such that I do not need to do anything on the device that needs to be joined(no button press or anything).
So far I've used ZDO_MGMT_DIRECT_JOIN_REQ for doing so. With this command the device that needs to be joined gets assigned a short address and also comes in the association list of my coordinator but still I could not control it by sending commands. I still need to press the button from the device to be joined. It(device to be joined) then sends ZDO_END_DEVICE_ANNCE_IND and only after that I could control the device.
Regards
Prasoon