Part Number: LAUNCHXL-CC26X2R1
Hello,
I want to create a menu in the CC2652 acting as a coordinator on the network.
The menu consist in these options:
1. Pair with another launchpad (end device or router)
2. List the bulbs availables and choose one to pair.
3. Set the configuration of a sensor (like a presence or temperature sensor)
Can be done?
The coordinator when we press <Commission> on the GUI creates the network, open the network and find devices who can join it. But that is way I do not know if it is possible because it is the bulb or the end device which joins the network. Can the coordinator choose which device to pair?
Thank you.