Part Number: CC2538EMK
Other Parts Discussed in Thread: CC2538, , Z-STACK
I am trying to decrease the receiver sensitivity of a node. Ryan Brown1 suggested here that I focus on the CCA threshold to be able to do it. But the problem is that even when I set the threshold, say -20, using RFCORE_XREG_CCACTRL0 = 0x35 knowing that CC2538_RSSI_OFFSET is -73, the device still gets packets with RSSI lower than -20 (e.g. -76). i.e. no change happens. I also tried that with the 4 CCA modes (0,1,2,3) but still the same.
I am using different firmware (RIOT-OS installed in Openmote-CC2538, CC2538EMK devices) and I am sure there is more than setting CCA value to make it work such as setting the RFCORE_XREG_RFC_OBS_CTRL0/1 with the right values. I also tried to map settings in your Zigbee firmware but I could not succeed to enable CCA.
I would really appreciate your input on the matter.
Here are some of the codes/definitions for the CC2538 module in RIOT-OS for your reference:
cc2538-rf.h
/**
* @brief Values for use with CCTEST_OBSSELx registers.
*/
enum {
rfc_obs_sig0 = 0,
rfc_obs_sig1 = 1,
rfc_obs_sig2 = 2,
};
/**
* @brief Values for RFCORE_XREG_RFC_OBS_CTRLx registers.
*/
enum {
constant_value_0 = 0x00, /**< Constant value 0 */
constant_value_1 = 0x01, /**< Constant value 1*/
rfc_sniff_data = 0x08, /**< Data from packet sniffer. Sample data
on rising edges of sniff_clk.*/
rfc_sniff_clk = 0x09, /**< 250kHz clock for packet sniffer data.*/
rssi_valid = 0x0c, /**< Pin is high when the RSSI value has
been updated at least once since RX was
started. Cleared when leaving RX.*/
demod_cca = 0x0d, /**< Clear channel assessment. See FSMSTAT1
register for details on how to configure
the behavior of this signal. */
sampled_cca = 0x0e, /**< A sampled version of the CCA bit from
demodulator. The value is updated whenever
a SSAMPLECCA or STXONCCA strobe is issued.*/
sfd_sync = 0x0f, /**< Pin is high when a SFD has been received
or transmitted. Cleared when leaving
RX/TX respectively. Not to be confused
with the SFD exception.*/
tx_active = 0x10, /**< Indicates that FFCTRL is in one of the TX
states. Active-high.*/
rx_active = 0x11, /**< Indicates that FFCTRL is in one of the
RX states. Active-high. */
ffctrl_fifo = 0x12, /**< Pin is high when one or more bytes are
in the RXFIFO. Low during RXFIFO overflow. */
ffctrl_fifop = 0x13, /**< Pin is high when the number of bytes
in the RXFIFO exceeds the programmable
threshold or at least one complete
frame is in the RXFIFO. Also highduring
RXFIFO overflow. Not to be confused with
the FIFOP exception.*/
packet_done = 0x14, /**< A complete frame has been received.
I.e., the number of bytes set by the
frame-length field has been received.*/
rfc_xor_rand_i_q = 0x16, /**< XOR between I and Q random outputs.
Updated at 8 MHz.*/
rfc_rand_q = 0x17, /**< Random data output from the Q channel
of the receiver. Updated at 8 MHz.*/
rfc_rand_i = 0x18, /**< Random data output from the I channel
of the receiver. Updated at 8 MHz */
lock_status = 0x19, /**< 1 when PLL is in lock, otherwise 0 */
pa_pd = 0x20, /**< Power amplifier power-down signal */
lna_pd = 0x2a, /**< LNA power-down signal*/
disabled = 0xff, /**< disabled */
};
/**
* @name RF CORE observable signals settings
*/
#ifndef CONFIG_CC2538_RF_OBS_0
#define CONFIG_CC2538_RF_OBS_0 tx_active
#endif
#ifndef CONFIG_CC2538_RF_OBS_1
#define CONFIG_CC2538_RF_OBS_1 rx_active
#endif
#ifndef CONFIG_CC2538_RF_OBS_2
#define CONFIG_CC2538_RF_OBS_2 rssi_valid
#endif
/* Default configuration for cc2538dk or similar */
#ifndef CONFIG_CC2538_RF_OBS_SIG_0_PCX
#define CONFIG_CC2538_RF_OBS_SIG_0_PCX 0 /* PC0 = LED_1 (red) */
#endif
#ifndef CONFIG_CC2538_RF_OBS_SIG_1_PCX
#define CONFIG_CC2538_RF_OBS_SIG_1_PCX 1 /* PC0 = LED_2 (red) */
#endif
#ifndef CONFIG_CC2538_RF_OBS_SIG_2_PCX
#define CONFIG_CC2538_RF_OBS_SIG_2_PCX 2 /* PC0 = LED_3 (red) */
#endif
#if ((CONFIG_CC2538_RF_OBS_SIG_2_PCX > 7) || \
(CONFIG_CC2538_RF_OBS_SIG_1_PCX > 7) || \
(CONFIG_CC2538_RF_OBS_SIG_0_PCX > 7))
#error "CONFIG_CC2538_RF_OBS_SIG_X_PCX must be between 0-7 (PC0-PC7)"
#endif
cc2538-rf.c
/**
* @name RF CORE observable signals settings
* @{
*/
#define CONFIG_CC2538_RF_OBS_SIG_0_PCX 5 /* PC5 */
#define CONFIG_CC2538_RF_OBS_SIG_1_PCX 6 /* PC6 */
#define CONFIG_CC2538_RF_OBS_SIG_2_PCX 7 /* PC7 */
/** @} */
static void _cc2538_observable_signals(void)
{
/* Select on which pin PC0:7 should the selected observable signals
be wired through, the signal is selected in CONFIG_CC2538_RF_OBS_%
and the pin in CONFIG_CC2538_RF_OBS_SIG_%_PCX */
if (IS_USED(MODULE_CC2538_RF_OBS_SIG)) {
if (CONFIG_CC2538_RF_OBS_0 != disabled) {
RFCORE_XREG_RFC_OBS_CTRL0 = CONFIG_CC2538_RF_OBS_0;
*(&CCTEST_OBSSEL0 + CONFIG_CC2538_RF_OBS_SIG_0_PCX) = \
CCTEST_OBSSELX_EN | rfc_obs_sig0;
}
if (CONFIG_CC2538_RF_OBS_1 != disabled) {
RFCORE_XREG_RFC_OBS_CTRL1 = CONFIG_CC2538_RF_OBS_1;
*(&CCTEST_OBSSEL0 + CONFIG_CC2538_RF_OBS_SIG_1_PCX) = \
CCTEST_OBSSELX_EN | rfc_obs_sig1;
}
if (CONFIG_CC2538_RF_OBS_2 != disabled) {
RFCORE_XREG_RFC_OBS_CTRL2 = CONFIG_CC2538_RF_OBS_2;
*(&CCTEST_OBSSEL0 + CONFIG_CC2538_RF_OBS_SIG_2_PCX) = \
CCTEST_OBSSELX_EN | rfc_obs_sig2;
}
}
}
void cc2538_init(void)
{
/* Enable RF CORE clock in active mode */
SYS_CTRL_RCGCRFC = 1UL;
/* Enable RF CORE clock in sleep mode */
SYS_CTRL_SCGCRFC = 1UL;
/* Enable RF CORE clock in PM0 (system clock always powered down
in PM1-3) */
SYS_CTRL_DCGCRFC = 1UL;
/* Wait for the clock enabling to take effect */
while (!(SYS_CTRL_RCGCRFC & 1UL) || \
!(SYS_CTRL_SCGCRFC & 1UL) || \
!(SYS_CTRL_DCGCRFC & 1UL)
) {}
/* Register Setting updates for optimal performance, RM section 23.15 */
RFCORE_XREG_TXFILTCFG = 0x09;
RFCORE_XREG_AGCCTRL1 = 0x15;
RFCORE_XREG_FSCAL1 = 0x01;
ANA_REGS_IVCTRL = 0x0B;
/* Enable AUTOCRC and AUTOACK by default*/
RFCORE_XREG_FRMCTRL0 = AUTOCRC | AUTOACK;
/* Disable RX after TX, let upper layer change the state */
RFCORE_XREG_FRMCTRL1 = 0x00;
/* Disable source address matching and pending bits */
RFCORE_XREG_SRCMATCH = 0x00;
/* Set FIFOP_THR to its max value*/
RFCORE_XREG_FIFOPCTRL = CC2538_RF_MAX_DATA_LEN;
/* Set default IRQ */
cc2538_rf_enable_irq();
/* Enable all RF CORE error interrupts */
RFCORE_XREG_RFERRM = STROBE_ERR | TXUNDERF | TXOVERF | \
RXUNDERF | RXOVERF | NLOCK;
_cc2538_observable_signals();
#ifdef CC2592_EMBEDDED
#if (CC2592_EMBEDDED == 1)
RFCORE_XREG_RFC_OBS_CTRL0 = 0x6A; //0x20; //0x6A;
RFCORE_XREG_RFC_OBS_CTRL1 = 0x68; //0x2a; //0x68;
#else
RFCORE_XREG_RFC_OBS_CTRL0 = 0x20; //0x20; //0x6A;
RFCORE_XREG_RFC_OBS_CTRL1 = 0x2a; //0x2a; //0x68;
#endif
CCTEST_OBSSEL2 = 0x80;
CCTEST_OBSSEL3 = 0x81;
#endif
/* Remaingin Code... */
}
With openmote-cc2538 normally the following registers have the following values
RFCORE_XREG_RFC_OBS_CTRL0 = 0x10;
RFCORE_XREG_RFC_OBS_CTRL1 = 0x11;
I tried to change them to the following to enable cca:
RFCORE_XREG_RFC_OBS_CTRL0 = 0x10;
RFCORE_XREG_RFC_OBS_CTRL1 = 0x0d; // also 0x0e
Please help,
Ahed