Other Parts Discussed in Thread: CC2530, Z-STACK
Hello,
I'm using the CC2530 module to form a SE Zigbee network. I am also using the the SampleApp aplication but I have really significant problems.
1. The coordinator starts the network and wait for new device announcements.
2. A new ZR router device successfully joins the network. When a new device (ZR again) joins the network, it seems it replaces the old one and steals its
short network address. I can see both announcements of the two devices, but I can not understant why this happens.
3. I have the same problem if two ZED devices are trying to join the network.
4. When I add two ZR and two ZED only one router and one end-device can join the network. (I observed the frames with packet sniffer)
Zigbee Pro is the selected stack profile, and the device addressing obeys to the stochastic algorithm for the nwk address assignment.
I really appreciate any response that could help me.
Thank you in advace