This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: OTA example stuck in reset

Part Number: CC2652R

Good morning,

I was experimenting your OTA example(zr_sw_ota_client). However, I am facing a problem with the reset. After the MCU reset being trigged, the MCU stuck in the boot (image 1 and 2).

 

(Image 1 and 2): Board reset stack.

 

Regarding, the MCU configuration of your OTA example, the instruction m3Hwi.resetVectorAddress change the reset vectors from address 0x00 to the address 0xA8(image 3 and 4).

(Image 3 and 4): Reset vectors address configuration and reset vectors address memory print.

After some analysis to the disassembly, I found that the reset vector address load to the program counter is from the address 0x04 (image5), and not from the address 0xA8. This results in a jump to a wrong memory address(image 6), resulting in the board reset.

 

 

(Image 5 and 6): Boot disassembly and PC after brunch instruction.

Could you help resolve this issue?