Part Number: CC2533
Team-
The logic input 1 on the CC2533 appears to be 2.5V from the data sheet. This seems quite high for a 3.3V IC. Is this correct? We would expect something closer to 2V?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2533
Team-
The logic input 1 on the CC2533 appears to be 2.5V from the data sheet. This seems quite high for a 3.3V IC. Is this correct? We would expect something closer to 2V?

Hello Antenna_Head,
This is the DC characteristic evaluated at VDD = 3 V and is the same parameter value reflected in the datasheet of any CC253X device. The hysteresis is within ±0.5 V of the target voltage for these devices.
Regards,
Ryan