Other Parts Discussed in Thread: Z-STACK
Hi,
I've bought a NodeOn Roller Shutter Node and everything works fine. (Link To It)
My only question is: when I plug the relay I receive a 0x4481 Message with ClusterID 0x1000. Looking at ZigBee Cluster PDF I cant seem to understand
Also: Do you think there is any way to get an input from the relay node regarding the percentage of roller shutter and so on. I've binded with 0x102 but nothing.
fe 27 44 81 0 0 0 10 a 4d 1 1 0 cc 0 37 4 46 0 0 13 9 1 40 7 b2 a4 fe ff ea 35 90 a 4d 1 4 1 2 2 1 a 4d 1d 10
Edit: Looking at the clusters in input:
<RX>11:52:31.72 COM4 ZDO_SIMPLE_DESC_RSP (0x4584)
SrcAddr: 0x581D
Status: ZDP_SUCCESS (0x0)
NwkAddr: 0x581D
Len: 0x18
Endpoint: 0x01
ProfileID: 0x0104
DeviceID: 0x0202
DeviceVersion: 1 (0x1)
NumInClusters: 0x07
InClusterList: 0x0000, 0x0003, 0x0004, 0x0005, 0x0102, 0x1000, 0xFC57
NumOutClusters: 0x01
OutClusterList: 0x0019
What kind of device ID is 0x0066? Can I find a complete list online?
<TX>11:56:36.72 COM4 ZDO_SIMPLE_DESC_REQ (0x2504)
DstAddr: 0x581D
NWKAddrOfInterest: 0x581D
Endpoint: 0xF2
<RX>11:56:36.73 COM4 ZDO_SIMPLE_DESC_REQ_SRSP (0x6504)
Status: afStatus_SUCCESS (0x0)
<RX>11:56:36.74 COM4 ZDO_SIMPLE_DESC_RSP (0x4584)
SrcAddr: 0x581D
Status: ZDP_SUCCESS (0x0)
NwkAddr: 0x581D
Len: 0x0C
Endpoint: 0xF2
ProfileID: 0xA1E0
DeviceID: 0x0066
DeviceVersion: 1 (0x1)
NumInClusters: 0x01
InClusterList: 0x0021
NumOutClusters: 0x01
OutClusterList: 0x0021
Best Regards,
Luca Vetri