Other Parts Discussed in Thread: CC2591, CC2530, Z-STACK
Hi All,
I'd like to program CC2530+CC2591 for personal use: make it listen to a CC2530 GPIO PIN and expose it as a "switch" through Zigbee. Simple, huh? Not for a novice like me.
I installed "IAR EW IDE - 8051", as well as "Z-Stack 3.0.2". I thought I would start with the "SampleSwitch" sample app, but it requires the EB. And I don't need EB with its LCD menu and stuff. I just need to produce a "hex" firmware which I can flash to my CC2530 and control through Zigbee rather than through the EB.
Any hints which sample app to use for quick start would be welcome!