Part Number: LP-CC2652RB
Other Parts Discussed in Thread: CC2652RB
.. is there an "easy" way to "configure" or "modify" the existing NCP example project to act as an RCP one?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-CC2652RB
Other Parts Discussed in Thread: CC2652RB
.. is there an "easy" way to "configure" or "modify" the existing NCP example project to act as an RCP one?
Hi,
By when would you need an RCP?
We plan to have this example ready for Q2 SDK (6.20), ETA 1st/2nd week of July.
If you need an RCP beforehand, I have a "local" approach for CC1352P2 RCP which may be referenced. It is on 5.30 SDK.
Please reach out if that interests you.
Thanks,
Toby
Thanks for reaching out toby!
I need an RCP firmware for the CC2652RB chip.
We would use our dongle (using the CC2652RB) for an OpenThread border router.
In particular for this homeassistant addon: https://github.com/home-assistant/addons-development/tree/master/openthread_border_router
But in general it would be great to use it for any other border-router that requires an RCP instead of an NCP..
Great to hear that you are working on that topic already!
Would be great if you could just attach a binary, out or elf file for me! Really appreciate that!
I was about to try this here: https://openthread.io/guides/build/index.md
By using this implementation: https://github.com/openthread/ot-cc13x2-cc26x2
but I couldnt find the time, even though I am not sure if it would work at all cause of the RB version of the chip? =)
Thanks, Sascha
Ok, here is something I put together. (I performed a simple ping test).
Please note that this should be used for evaluation purposes only, the SDK-release quality version of RCP will be available in 6.20 SDK.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/158/rcp_5F00_LP_5F00_CC2652RB_5F00_tirtos_5F00_gcc.out
Insane Toby, as usual!
Thank you, yes sure, I will use it only for testing purposes!
Cant wait to see the next SDK update