Part Number: CC2531EMK
Other Parts Discussed in Thread: CC2531, Z-STACK, CC2530
Hi all,
I am working on a set of custom PCBs that both use CC2531, designed to be both sensor/data accumulator and coordinator.
I am trying to compile the example ZNP project from Z-Stack 3.0.2 with the UART enabled so we can get some debug output, and having a bit of a nightmare.
Changing the #define in hal_board_cfg.h so HAL_UART_ISR is 1 and HAL_UART_USB is 0 causes a compilation error due to lack of _hal_uart_isr.c, a quick search shows it in $ZSTACK_DIR\Components\hal\target\CC2350ZNP, so I've added this include directory to project options, but now have a missing definition for HAL_UART_PRIPO in the newly included c file.
Another search and the definition can be found in hal_board_cfg.h in the same \Components\hal\target\CC2530ZNP folder, but the CC2531 - Debug project options don't appear to reference the include by name, so I added it to the top of _hal_uart_isr.c, but the definition was still not picked up.
At this point I wonder if I am barking up the wrong tree, is it possible (within reason) to route the UART out from this chip while making use of the ZNP example project?
Thanks,
Will