Other Parts Discussed in Thread: CC2530
Hi All,
I am new to MSP430 because I am currently using the Microchip's PI24/32 and considering going to TI based hardware en software.
I want to build a remote sensing application using a CC2530 Remote Sensing board in combination with a device that has 1-Wire and I2C interfaces and an analog output signal. Can I connect that device to the MSP via the header on the CC2530 remote sensor module with the following schematics:
http://www.rlocman.ru/i/File/2011/01/10/CC2530_ZNP_Schematic.pdf
Many thanks in advance,
Cheers
André