Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: Heartbeat/SYS_PING Required?

Part Number: LAUNCHXL-CC26X2R1

Hello,

I let my network run for some time. I observed that the communication does "freeze" sometimes. I need to restart my script. Right now, I do not know exactly where the problem is as I am using a USR-TCP232-T2 to connect the LAUNCHXL-CC26X2R1 to the network.

There is very little if not no data at all from my 2 sensors over night within a timeframe of 2 hours. Sometimes the sensor sends some message indicating the battery level.

I just want to make sure, if there is maybe some heartbeat required, like a SYS_PING command from time to time to prevent the device from "freezing up". Again, I am not sure if the LAUNCHXL-CC26X2R1 is freezing or if it is the connection to the network (USR-TCP232-T2).

Any other idea what could be the issue?

Regards,

Robert