This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630: Crystal 32.768kHz alternatives for an existed design

Part Number: CC2630

Hello Team,

We need your help on our customer's concern below. Here is the question below.

 We have a question regarding using different suppliers of a 32,768kHz crystal in an existed design for CC2630. As we are willing to extend the suppliers list for the 32.768kHz crystal..

We wanted to ask you kindly to support us with your opinion based on your experience on whether the second source crystals are suitable to be used for CC2630 ZigBee or not. The crystal comparison sheet will be listed as follows:

 

 

[Original Part]FC-135 32.7680KA-AG0

ABS07-32.768kHz-7-T

830108488401 (LFXTAL084884)

X1A000161xxxx16 (FC3215AN 32.768000 7 +20.0-20.0)

 

Manufacturer

Seiko-Epson

ABRACON

Wurth Elektronik GmbH

Seiko Epson

Package (mm)

3.2L * 1.5W

(mm)

3.2L * 1.5W

(mm)

3.2L * 1.5W (mm)

3.2L * 1.5W

(mm)

Frequency

32.768 kHz

32.768 kHz

32.768 kHz

32.768 kHz

Frequency Tolerance (ppm)

± 20

± 20

± 20

± 20

Operating temperature

-40°C to +85°C

-40°C to +85°C

--------------------

-40°C to +105°C

Turnover Temperature

+20°C to +30°C

+20°C to +30°C

+20°C to +30°C

+25 ± 5

Load Capacitance

7 pF

7 pF

7 pF

7 pF

Shunt Capacitance

1 pF

1.2 pF

1.5 pF

1.6 pF

Series Resistance (Ω)

70K

70K

70K

50K

Aging (ppm)

±3

±3

±3

±3

Data sheets

Datasheet

Datasheet

Datasheet

Datasheet

Furthermore, We were checking the specification of the CC2630 if the alternative crystals are a good fit. Luckily the alternatives seem within TI requirements as was mentioned in the datasheet.

Thank you so much in advance.

Best regards,

Jonathan