Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
SDK:z-stack home 1.2.2.a.44539
It is described in 3.6.10.4 MAC data poll processing in the R21/2015 specification that if there is no corresponding entry in the neighbor table, a leave message should be sent.
cc2530 is the coordinator, and an end device is associated with this coordinator. When AssocRemove() is used to delete the association table entry corresponding to the end device,
the coordinator will continue to respond to the end device's mac data poll by capturing packets, which is inconsistent with the protocol specification.
This is why?