This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Some problems about Firmware(SmartRF04EB) + ZStack-CC2530-2.4.0-1.4.0

Other Parts Discussed in Thread: CC2430, Z-STACK, CC2530

HI,

   i have some problems about Firmware(SmartRF04EB) + ZStack-CC2530-2.4.0-1.4.0.

   my program EB's rev is SmartRF04EB(0042),that i used to download hex in CC2530-2.3.1 and cc2430.

   Is my program EB can be used to download the hex from CC2530-2.4.0-1.4.0?

   Because i find some problem in uart when i download whit SmartRF04EB(hex is 2.4.0),it doesn't work.But the uart work correctly if i download the hex in CC2530-2.3.1.

   And why i can't update EB Firmware whit Setup_SmartRFProgr_1.11.1?

  my program EB is C8051 + Firmware(SmartRF04EB),i do it myself.

Thanks in advance

  • Hi,

    I would recommend to use a SmartRf05EB for CC2530 and Z-stack, instead of the SmartRf04EB.

    SmartRF05EB + CC2530 is the platform that Z-stack support. See also "Z-Stack User's Guide - CC2530DB.pdf" and "Getting Started Guide - CC2530.pdf" for more information.

    With regards,

    Bjørn