Part Number: CC2430
We use CC2430 for customized product. The only radio change we did comparing to standard ZigBee is as below:
SYNCWORDL = 0x0B;
SYNCWORDH = 0xE4;
//[ preamble][sync ]
//[00][00][00][0B][E4]
I have an issue configurating Silicon Labs chip to receive your packet. We tried a lot of things without succes.
On things which came into our mind was what are the settings for DSSS in CC2430. Here is screenshot what I can set in SL chip:

SL support didn't succeed yet, hence they tried decode RF raw data and had beginning 0x00 0x00 0x00 0x0A matched symbols (with DSSS Chipping Code Base as in the picture)
, but the rest doesn't match patterns.
Can anyone help with this issue?
Thanks!