This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: cc1352P1 Launchpad flashing but not executing.

Part Number: CC1352P
Other Parts Discussed in Thread: UNIFLASH, SIMPLELINK-CC13XX-CC26XX-SDK, , CC1350

Hi

I am trying to use CC1352P1 for my thread  PoC, and I observer that board is getting flashed with proper output file using Uniflash.

But I don’t see program executing,

 I could compile and build the project using CCS.  Flashed the output file of LED blink examples, and I don’t see that program is running.

 The two CC1352P1 are exhibiting the same behavior, looks like i am missing some settings, can some one help me on this.

Thanks

Uniflash_screenshot.docx