Part Number: CC2530
Hi team,
Here's the request from the customer:
Customer configured the pins of the two IOs of the debug port as inputs. When the device is working, these two pins will have high and low level inputs.
Customer found that the code is formatted for unknown reason after running the project. Would it enter the debug mode in a certain state?
Is there any way to solve it without modifying hardware?
Could you help check this case?
Thanks. Best Regards,
Nick