Part Number: CC2652R7
Hi team,
I follow up below link to setup Matter environment for CC2652R7. Please instruct what are the value for target_os and target_cpu ? Thank you.
--> overall: https://github.com/project-chip/connectedhomeip/blob/master/docs/guides/BUILDING.md
Build custom configuration
The build is configured by setting build arguments. These are set by passing the --args option to gn gen, by running gn args on the output directory, or by hand editing args.gn in the output directory. To configure a new build or edit the arguments to existing build, run:
source scripts/activate.sh
gn args out/custom
ninja -C out/custom
Two key builtin build arguments are target_os and target_cpu, which control the OS & CPU of the build.