Hi,
I'm implementing an OTA Server.
When sending the OTA Image notify Command with the following fields:
- Frame Control: 0x09 (0b1001 so Frame Type equal to 01, manufacturer flag disabled, and default response not set because is unicast message)
- Payload Type = 0x02
- Query Jitter = 99
- Manufacturer Code = 0x1246 ( converted to 0x46 0x12)
- Image Type = 0x0100 ( converted to 0x00 0x01)
I receive an AF_DATA_CONFIRM from the device but I don't receive any OTA Answer.
Any possible cause of this?