Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Get LQI of End-Device.

Hi,

So I have the following setup:

  • Coordinator.
  • Repeater close to the coordinator.
  • End Device Far away from coordinator ( and repeater ) and connected to repeater.

To determine the LQI I use the LQI field in the AF_INCOMING_MSG, but I realized it gives the value of the last Hop.

Is there any way to get the overall LQI between the coordinator and end-device although it is connected to a repeater, or not?.

Best Regards,

Aiman Hammou