This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R7: Thread power consumption on standby

Part Number: CC2652R7

Hello

I am using CC2652 as a thread end device. have a scenario where the device will mostly be on standby. But it need to be always connected to the network so that I can receive commands. For Rx it uses approx. 6 mA current. How much current does it use when on standby, i.e., ready and able to receive?

Example - In one day, the device spends 10 seconds in total receiving data. The remaining time it is always connected to the network but just idle. Will it still consume 6 mA? Is there any way or strategy to reduce the current consumption?