This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: [Extreme Project][CC2652R1] How to modify 802.15.4 sample source ("cli_ftd" source) to support "normal mode" test for PASS Taiwan BSMI certification?

Part Number: CC2652R

Hi TI

we got [Extreme] MP project that it has to PASS Taiwan BSMI certification (802.15.4 authentication), the criteria has to use "normal mode" to setup and test "802.15.4", 

so, can you update information for support this test ?

my detail information:

1. chipset using "cc2652R1"

2. TI sample code use and download from "TI Resource Explorer -> CC26x2R LaunchPad -> TI Thread -> cli_ftd -> TI-RTOS -> CCS compiler -> cli_ftd"

3. For "normal mode", I used setup "peripheral role and enabled advertisement" HCI commands for BLE "normal mode" setup, that's work. (it used cell phone to scan BLE signal, it works)  (for example) 

so, how to use "cli_ftd" sample source to setup "802.15.4" normal mode ? 

(is need to modify "cli_ftd" sample source for support? or have any commands can setup to normal mode not "CTX" ?)

Thank you

WNC / Danny