Other Parts Discussed in Thread: CC2530
HIi,
I use the CC2530ZDK module to implement a ZigBee Device. So I will use the intern flash to save my sensors Data (16 Bytes in one day). I will reserv 2 Pages for this.
the 16 bytes can Be saved as structure or Array[16];
so how can I reserv 2 Pages to only save this data (reserv code or varaibles to use this Pages).
this reserved pages of the flash should be errased by Programming. Then I will append the data until the 2 pages are ful from data so I can re-errase it to begin from the firs Adress inthis Pages.
Any API Funktion to do this? and examples ?