Part Number: CC2531
Hi,
Iam try to control the loads via ztool using 4 load switch when i control the single load but other load are turns on. i check the AF data Request command single load is sended.
Start Time: 12/17/2022 3:12:14 PM
<TX>03:13:35.27 COM6 AF_DATA_REQUEST (0x2401)
DstAddr: 0xFC5A
DestEndpoint: 0x03
SrcEndpoint: 0x01
ClusterID: 0x0006
TransID: 0x01
Options: 0x02
Radius: 0x07
Len: 0x03
Data: ... (0x01, 0x01, 0x00)
<RX>03:13:35.28 COM6 AF_DATA_REQUEST_SRSP (0x6401)
Status: afStatus_SUCCESS (0x0)
<RX>03:13:35.28 COM6 AF_DATA_CONFIRM (0x4480)
Status: afStatus_SUCCESS (0x0)
Endpoint: 0x01
TransID: 0x01
<RX>03:13:35.39 COM6 ZDO_SRC_RTG_IND (0x45C4)
DstAddr: 0xFC5A
Relay Count: 0x00
Relay List
<RX>03:13:35.41 COM6 AF_INCOMING_MSG (0x4481)
GroupID: 0x0000
ClusterID: 0x0006
SrcAddr: 0xFC5A
SrcEndpoint: 0x03
DstEndpoint: 0x01
WasBroadcast: 0x00
LinkQuality: 0x59
SecurityUse: 0x00
Timestamp: 0x003683DE
TransSeqNumber: 0x00
Len: 0x05
Data: ..... (0x08, 0x01, 0x0B, 0x00, 0x00)