Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: RF front end External BIAS + BALUN

Part Number: CC2652P

Hi TI!

I am using the CC2652P with the2450BM14G0011 balun for the 2.4GHz differential output so the bias for the LNA is internal. If I want to change the LNA bias to external, using the same balun (2450BM14G0011), the schematic should look like the following one? Or better keep it with internal bias?

Thank you very much.