Part Number: CC2652R
Hi
We are observing an when sometimes we get a chain of 'Many to one failures' from the router device to the coordinator and sometimes this goes into 1000s of message, have seen a case where it went to 9000 messages on the sniffer (took a few minutes to stop, not sure why it did either)
This was observed when the device was far away from the coordinator and wasn't getting a MAC ack.
Not sure why this is happening, is there anyway I can limit these messages.
Few of the network parameters
1. Many to one to ZNP coordinator triggered every 255 seconds
2. Route expiry disabled on Routers.
3. Large network 100+ devices.
Any advise would be helpful. Please let me know if you need any further information.
Thanks
Akhilesh