This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IAS_ZONE_ENROLL_REQUEST via sniffer but not via Serial Port.

Hi,

I'm implementing this smoke alarm into our system. 

After writing the IEEEAddress to the Attribute 0x0010 in the IAS_ZONE Cluster, I see via Sniffer that I receive a IAS_ZONE_ENROLL_REQUEST but can't see it via Serial Port.

Maybe I have to add a flag to the znp_cnf.opts file?

Also: to call a cluster specific command what value does the field control need to have?