Other Parts Discussed in Thread: CC1352P,
Dear Sir and Madam,
A custom CC1352P Module was design based on CC1352P_2_LAUNCHXL, SubGHz:14dBm and 2.4GHz :19dBm.
wireless MCU CC1352P was replace by CC1352P7 in this custom board only.
There was no LP-CC1352P2-2 , following 2 launchpad were available
- LP-CC1352P7-1: 868/915 MHz up to 20 dBm, 2.4 GHz up to 5 dBm
- LP-CC1352P7-4: 433 MHz up to 13 dBm, 2.4 GHz up to 10 dBm
Which example is best fit CC1352P_2_LAUNCHXL application power distribution and what should be change (e.g. RF Antenna Pin 0,1,2) ?
Best regards,
David