This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

.Net framework configuration error when installing ZStack-CC2430-1.4.3-1.2.1

Dear all, two months ago I could properly install the  ZStack-CC2430-1.4.3-1.2.1 on window XP.  Today I reinstalled my OS and installed the Visual Studio 2005 and Visual Studio 6.0. The VS6.0 was installed after the VS2005. Then the problem emerged. When I double click on the ZStack-CC2430-1.4.3-1.2.1.exe, the installing procedure was trapped in "configuring microsoft(r) .Net framework".

My OS is Windows XP SP3, both .Net framework1.1 Configuration icon and .Net framework2.0 Configuration icon are presented in the administrative tools of the control panel.

I desperately need your help ,thank you