Part Number: CC2530
Other Parts Discussed in Thread: CC2650, Z-STACK
Hi team,
Here's the request from the customer:
Currently using cc2650 as the zigbee terminal node, send 50 bytes of data to the coordinator cc2530
The coordinator CC2530 receives 50 bytes of data and transmits it to the computer with uart
The serial port of the computer can receive data.
But when the cc2650 wants to send 100 bytes of data, the computer serial port cannot receive the data.
Is it caused by the large amount of received data? What is the maximum number of bytes of received data?
Is the size of the data received by the zigbee coordinator configured by itself? How to modify the configuration file?
Could you help check this case? Thanks.
Best Regards,
Nick