This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: CC2530 Battery Monitoring function confirmation request[Mail reply request]

Part Number: CC2530

I am inquiring about the CC2530 IC.

The battery monitoring function is specified in DATASHEET, and I would like to know more about this.

Currently, a separate Battery Detect IC is used, but I want to do battery monitoring using the CC2530.

Battery 3.3V is used. (AA batteries 2EA)

I want to divide this part into 3 steps and detect it.

For example, High area (3.3~3.0V) / Middle area (2.9V~2.6V) / Low area (2.5V~2.2V)

I can't share the circuit diagram, so I would appreciate it if you could reply to my email.

ninedragonlee@osstem.com