This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bind Status Code: Not Supported.

Hi,

.

I have this FYRTUR Roller Blind and his remote.

I'm sending a bind between the remote and the shutter so I can control the roller blind via Remote.

Using CC2562P Dongle.

.

DstAddr --> Nwk Address of the remote

srcAddr --> IEEE Address of the remote

srcEP --> endpoint of remote

clusterID --> 0x0102 (Window Covering Cluster)

bindAddr --> IEEE Address of shutter

dstEP --> endpoint of shutter

I'm trying to bind the cluster 0x0102 which should be implemented on both devices.

Here is the log. The key is: 0xaabbccddeeff00112233445566778899

Packet number 330.

BindNorSupported.rar