This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: json file not found

Part Number: CC2652P
Other Parts Discussed in Thread: CCSTUDIO, , SIMPLELINK-CC13XX-CC26XX-SDK, , SYSCONFIG, CC2652RB

 There is an example empty project imported from Resource Explorer, CC1352-P-2. I tried to switch the device to several custom boards, all of them works; for example CC1352P1F3RGZ. The only one so far what does not seem to be working is the CC2652P1FRGZ one. The error message says /ti/ti154stack/rf_config-/CC2652P1FRGZ_rf_defaults.js is not found. The file system contains several copies of CC2652P1FRGZ_rf_defaults.js so my question is why the latest CCStudio does not find this file after a fresh installation? Does this file need to be copied somewhere? Or, if not, which PATH/environment variable needs to be adjusted in order to be able to switch to CC2652P1? It is really annoying because the switch to none/device works for everything else I tried in CCStudio.