Part Number: CC1352P
Other Parts Discussed in Thread: SIMPLELINK-CC13XX-CC26XX-SDK, Z-STACK, ,
Hello,
Customer is using the z-stack which is part of SIMPLELINK-CC13XX-CC26XX-SDK, version 6.40.00.13. it is zigbee 3.0 technology.
They have four questions for Texas. All questions are from the CC1352P, using the LAUNCHXL-CC1352P1 development board.
1- Within the zigbee "z-stack" protocol, is there any way to change the role of the device, for example from coordinator to router, using the same programming code or does there always have to be three versions, one for coordinator, router and end device?
2- SIMPLELINK-CC13XX-CC26XX-SDK, inside the example codes in the z-stack folder, there is information to change the configuration like PAN ID, Channels, Short Addresses, any configuration parameters through AT commands ?
3- They are performing the functional tests using the example codes:
- Zigbee Coordinator Light Example App/ Zigbee Router Switch Example App
- Zigbee Coordinator Door Lock Example App/ Zigbee Router Door Lock Controller Example App
- Zigbee Coordinator Thermostat Example App/ Zigbee Router Temperature Sensor Example App
These example codes are basic, does TI happen to have any production test oriented code with zigbee communication?
4 - Is there any document that explains the process of configuring variables such as PAN ID, Channels, Short Addresses, Status, etc., for the z-stack that is part of SIMPLELINK-CC13XX-CC26XX-SDK?
thanks and Best Rgds
Raphael Marchi - TI FAE