Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC2652RB: DEVICE JOINED, NOT ANSWERING PING PACKETS.

Part Number: LP-CC2652RB
Other Parts Discussed in Thread: CC1352P

It’s some months we’re working quite fine on a ZigBee project  developed on CCS  studio, “zr_genericapp_CC1352P_2_LAUNCHXL_tirtos_ticlang”  (thanks a lot to Mr. Ryan who supported us each time we were on troubles…)

 Each one of our router/end devices is configured with 8+1 endpoints and we handle all our devices (at the moment) with Zigbee2Mqtt application….

 At main task application “zcl_genericapp.c” file, we continuously check the “bdbAttributes.bdbCommissioningStatus” to be   “BDB_COMMISSIONING_SUCCESS”  or “BDB_COMMISSIONING_NETWORK_RESTORED”, to see wether the device is joined on the network or not...

I hoped this was enough to be sure the device was joined to network;  but after some days of continuous testing (4 routers+16 end devices),  this morning I found a device not responding to network commands:

At Zigbee2Mqtt level I see it as the message “… failed to ping …device” repeatedly appearing!  Even switching ON/OFF attributes of each end device, nothing happens.

Please consider that an associated LED on our target is blinking in such a way, telling me that “bdbAttributes.bdbCommissioningStatus” matches the above two values. So I really don’t know what other check I have to do to be sure the device is capable to handle endpoints R/W attributes!

Here is the question: could be enough checking  the periodic incoming PING packet from coordinator? (without the needs of adding application level commands….sent from coordinator )

If so, what function call or variable check can I do for this purpose?

 

Thanks a lot

Roberto

  • Hi Roberto,

    BDB_COMMISSIONING_NETWORK_RESTORED is only intended for ZG_BUILD_ENDDEVICE_TYPE who have lost their parent device, and  BDB_COMMISSIONING_SUCCESS could refer to any bdbCommissioningMode (Initialization, Formation, Steering, F&B).  You could instead check the zstack_DevState (should be zstack_DevState_DEV_END_DEVICE or zstack_DevState_DEV_ROUTER) or bdbAttributes.bdbNodeIsOnANetwork (should be TRUE). 

    Beyond that, I suggest you debug a faulty device to determine what state it is operating under.  If it is still receiving, ACKing, and responding to neighbor devices on the network then it is still connected.  A ZED which is not polling often enough may miss some ping packets and still be joined (i.e. has not been aged out yet).

    Regards,
    Ryan