Part Number: CC1352P7
Other Parts Discussed in Thread: UNIFLASH, , Z-STACK, CC2652R7
HI TI!!
I'm trying to load from the CCS a firmware from examplo zr_sw_ota ... (any example the same result) after hitting RUN the MCU resets. If I load the .hex with uniflash, it does nothing after loading the firmeare.
In the project readme it says: This application also requires that the off-chip BIM application image is flashed alongside this project application's output .bin. I don't understand this.
In the output folder .hex, .out, .bin files are generated.
I have tried all combinations and I have no success.
So: What should I do to load an OTA firmware correctly?
Thank you very much! Best regards