This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: NVS Hot Item / APSME_SearchTCLinkKeyEntry

Part Number: CC2652R

Has anyone got a TIRTOS7 NVS hot item patch? Or perhaps a modified version of APSME_SearchTCLinkKeyEntry that is able to get reasonable performance on Zigbee 3.0 (only) networks. When dealing with Zigbee 3.0 Zstack is quite slow with a significant amount of time being taken up by NVS.

Related:

 - https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1057311/cc2652p-function-apsme_searchtclinkkeyentry-in-sdk-5-30-execute-wrong-result/3911553#3911553

 - https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1057307/cc2652p-hot-nv-item-on-zstack

  • Hi Mathew,

    You would need to consult on this topic given that the TI SDK does not implement the NVS hot item feature which they implemented.

    https://e2e.ti.com/f/1/t/1057307 
    https://e2e.ti.com/f/1/t/1200442 

    Regards,
    Ryan

  • For the first part of my query here is my attempt at the solution:

    diff --git a/znp_CC26X2R1_LAUNCHXL_tirtos_ccs/Application/Services/nvocmp.c b/znp_CC26X2R1_LAUNCHXL_tirtos_ccs/Application/Services/nvocmp.c
    index 802442d..9908941 100644
    --- a/znp_CC26X2R1_LAUNCHXL_tirtos_ccs/Application/Services/nvocmp.c
    +++ b/znp_CC26X2R1_LAUNCHXL_tirtos_ccs/Application/Services/nvocmp.c
    @@ -207,6 +207,9 @@ Requires API's in a crc.h to implement CRC functionality.
     #include "nv_linux.h"
     #endif
     
    +
    +#include  "zcomdef.h"
    +
     //*****************************************************************************
     // Constants and Definitions
     //*****************************************************************************
    @@ -521,6 +524,13 @@ typedef struct
         uint8_t  hpage; // Header page
     } NVOCMP_itemHdr_t;
     
    +typedef struct {
    +    uint32_t cmpid; // Compressed ID
    +    uint16_t subid; // Sub ID
    +    uint16_t itemid; // Item ID
    +    uint8_t  sysid; // System ID
    +} NVOCMP_hotItem_t;
    +
     // Length (bytes) of compressed header
     #define NVOCMP_ITEMHDRLEN  7
     
    @@ -638,6 +648,34 @@ typedef struct
       NVOCMP_compactInfo_t compactInfo;
       NVOCMP_pageInfo_t pageInfo[NVOCMP_NVPAGES];
     } NVOCMP_nvHandle_t;
    +
    +typedef struct
    +{
    +  bool     vail;
    +  uint8_t  pg;
    +  uint16_t ofs;
    +} NVOCMP_hotNv_t;
    +
    +#define   NVOCMP_HOT_IDS_ARRAY    { \
    +          {NVOCMP_CMPRID(NVINTF_SYSID_ZSTACK,ZCD_NV_EX_LEGACY,ZCD_NV_NWKKEY), {false, 0xFF, 0xFFFF}}, \
    +          {NVOCMP_CMPRID(NVINTF_SYSID_ZSTACK,ZCD_NV_EX_LEGACY,ZCD_NV_NWK_ACTIVE_KEY_INFO), {false, 0xFF, 0xFFFF}}, \
    +          {NVOCMP_CMPRID(NVINTF_SYSID_ZSTACK,ZCD_NV_EX_LEGACY,ZCD_NV_NWK_ALTERN_KEY_INFO), {false, 0xFF, 0xFFFF}}, \
    +          {NVOCMP_CMPRID(NVINTF_SYSID_ZSTACK,ZCD_NV_EX_LEGACY,ZCD_NV_TCLK_SEED), {false, 0xFF, 0xFFFF}}, \
    +           }
    +
    +typedef struct
    +{
    +  uint32_t cid;
    +  NVOCMP_hotNv_t nv;
    +} NVOCMP_hotId_t;
    +
    +
    +
    +NVOCMP_hotId_t NVOCMP_hotIdArray[] = NVOCMP_HOT_IDS_ARRAY;
    +
    +
    +
    +
     //*****************************************************************************
     // Local variables
     //*****************************************************************************
    @@ -695,6 +733,11 @@ static uint16_t NVOCMP_badCRCCount = 0;
     NVOCMP_initAction_t gAction;
     uint8_t NVOCMP_size;
     
    +NVOCMP_hotNv_t* (*pfn_nvocmp_hotItemMatch)(NVOCMP_hotItem_t hotItem) = NULL;
    +void (*pfn_nvocmp_hotItemUpdate)(uint8_t pg, uint16_t ofs, NVOCMP_hotItem_t hotItem) = NULL;
    +NVOCMP_hotNv_t* (*pfn_nvocmp_hotItemMatchCont)(uint8_t sysid, uint16_t itemid, void *cBuf, uint16_t clength, uint16_t coff) = NULL;
    +void (*pfn_nvocmp_hotItemUpdateCont)(NVOCMP_hotItem_t hotItem, void *cBuf, uint16_t clength, uint16_t coff) = NULL;
    +
     //*****************************************************************************
     // NV API Function Prototypes
     //*****************************************************************************
    @@ -777,6 +820,11 @@ static void       NVOCMP_migratePage(NVOCMP_nvHandle_t *pNvHandle, uint8_t page)
     static void       NVOCMP_copyItem(uint8_t srcPg, uint8_t dstPg, uint16_t sOfs, uint16_t dOfs, uint16_t len);
     #endif
     
    +static NVOCMP_hotNv_t* NVOCMP_hotItemMatch(NVOCMP_hotItem_t hotItem);
    +static void  NVOCMP_hotItemUpdate(uint8_t pg, uint16_t ofs, NVOCMP_hotItem_t hotItem);
    +static bool  NVOCMP_hotItemMatchCont(uint8_t sysid, uint16_t itemid, NVOCMP_itemInfo_t *pInfo, NVOCMP_itemHdr_t* pHdr);
    +static void  NVOCMP_hotItemUpdateCont(NVOCMP_hotItem_t hotItem, void *cBuf, uint16_t clength, uint16_t coff);
    +
     //*****************************************************************************
     // Load Pointer Functions (These are declared in nvoctp.h)
     //*****************************************************************************
    @@ -3156,6 +3204,14 @@ static void NVOCMP_writeItem(NVOCMP_nvHandle_t *pNvHandle, NVOCMP_itemHdr_t *pHd
             dLen = pHdr->len;
             hOfs = dstOff + dLen;
     
    +        // update hot ids, luoyiming 2020-05-22
    +        NVOCMP_hotItem_t hotItem = {.subid = pHdr->subid, .itemid = pHdr->itemid, .sysid = pHdr->sysid};
    +        hotItem.cmpid = pHdr->cmpid;
    +        NVOCMP_hotItemUpdate(dstPg, dstOff, hotItem);
    +
    +        // update cont hot id, luoyiming 2021-11-29
    +        NVOCMP_hotItemUpdateCont(hotItem, pBuf, pHdr->len, 0);
    +
             if (iLen <= NVOCMP_SMALLITEM)
             {
                 // Construct item in one buffer
    @@ -3649,6 +3705,51 @@ static int8_t NVOCMP_findItem(NVOCMP_nvHandle_t *pNvHandle, uint8_t pg, uint16_t
     #ifdef NVOCMP_GPRAM
         NVOCMP_disableCache(&vm);
     #endif
    +    // find hot id first, luoyiming 2020-05-21
    +    if( (flag & NVOCMP_FINDLMASK) == NVOCMP_FINDSTRICT )
    +    {
    +      NVOCMP_hotItem_t hotItem = {.subid = pHdr->subid, .itemid = pHdr->itemid, .sysid = pHdr->sysid};
    +      hotItem.cmpid = cid;
    +      NVOCMP_hotNv_t* pHotNv = NVOCMP_hotItemMatch(hotItem);
    +      if( pHotNv )
    +      {
    +        NVOCMP_itemHdr_t iHdr;
    +        NVOCMP_readHeader(pHotNv->pg, pHotNv->ofs, &iHdr, false);
    +        if((iHdr.stats & NVOCMP_ACTIVEIDBIT) &&
    +          !(iHdr.stats & NVOCMP_VALIDIDBIT))
    +        {
    +          if( iHdr.cmpid == cid )
    +          {
    +            memcpy(pHdr, &iHdr, sizeof(NVOCMP_itemHdr_t));
    +#ifdef NVOCMP_GPRAM
    +            NVOCMP_restoreCache(vm);
    +#endif
    +            return(NVINTF_SUCCESS);
    +          }
    +        }
    +      }
    +    }
    +    else if((pInfo) && ((flag & NVOCMP_FINDHMASK) == NVOCMP_FINDCONTENT))
    +    {
    +      if( pHdr->subid == 0 )
    +      {
    +        NVOCMP_itemHdr_t iHdr;
    +        if(true == NVOCMP_hotItemMatchCont(pHdr->sysid, pHdr->itemid, pInfo, &iHdr))
    +        {
    +          if(!NVOCMP_readItem(&iHdr, 0, pInfo->rlength, pInfo->rBuf, false))
    +          {
    +            if(!memcmp((uint8_t *)pInfo->rBuf + pInfo->coff, pInfo->cBuf, pInfo->clength))
    +            {
    +              memcpy(pHdr, &iHdr, sizeof(NVOCMP_itemHdr_t));
    +#ifdef NVOCMP_GPRAM
    +              NVOCMP_restoreCache(vm);
    +#endif
    +              return(NVINTF_SUCCESS);
    +            }
    +          }
    +        }
    +      }
    +    }
     
         for(p = pg; nvSearched < NVOCMP_NVSIZE; p = NVOCMP_DECPAGE(p), ofs = pNvHandle->pageInfo[p].offset)
         {
    @@ -3659,7 +3760,7 @@ static int8_t NVOCMP_findItem(NVOCMP_nvHandle_t *pNvHandle, uint8_t pg, uint16_t
             continue;
           }
     #endif
    -      NVOCMP_read(pg, 0, (uint8_t *)pTBuffer, FLASH_PAGE_SIZE);
    +      NVOCMP_read(p, 0, (uint8_t *)pTBuffer, FLASH_PAGE_SIZE);
     
           while(ofs >= (NVOCMP_PGDATAOFS + NVOCMP_ITEMHDRLEN))
           {
    @@ -3687,6 +3788,9 @@ static int8_t NVOCMP_findItem(NVOCMP_nvHandle_t *pNvHandle, uint8_t pg, uint16_t
                       if (cid == iHdr.cmpid)
                       {
                           found = true;
    +                      NVOCMP_hotItem_t hotItem = {.subid = iHdr.subid, .itemid = iHdr.itemid, .sysid = iHdr.sysid};
    +                      hotItem.cmpid = iHdr.cmpid;
    +                      NVOCMP_hotItemUpdate(p, ofs, hotItem);
                       }
                       break;
                   case NVOCMP_FINDSYSID:
    @@ -3719,8 +3823,14 @@ static int8_t NVOCMP_findItem(NVOCMP_nvHandle_t *pNvHandle, uint8_t pg, uint16_t
                     {
                       if(!NVOCMP_readItem(&iHdr, 0, pInfo->rlength, pInfo->rBuf, false))
                       {
    +                    // update hot item when read item success.
    +                    NVOCMP_hotItem_t hotItem = {.subid = iHdr.subid, .itemid = iHdr.itemid, .sysid = iHdr.sysid};
    +                    hotItem.cmpid = iHdr.cmpid;
    +                    NVOCMP_hotItemUpdate(p, ofs, hotItem);
    +
                         if(!memcmp((uint8_t *)pInfo->rBuf + pInfo->coff, pInfo->cBuf, pInfo->clength))
                         {
    +                      NVOCMP_hotItemUpdateCont(hotItem, pInfo->cBuf, pInfo->clength, pInfo->coff);
                           memcpy(pHdr, &iHdr, sizeof(NVOCMP_itemHdr_t));
     #ifdef NVOCMP_GPRAM
                           NVOCMP_restoreCache(vm);
    @@ -3797,6 +3907,46 @@ static int8_t NVOCMP_findItem(NVOCMP_nvHandle_t *pNvHandle, uint8_t pg, uint16_t
         uint16_t items = 0;
         uint32_t cid = NVOCMP_CMPRID(pHdr->sysid,pHdr->itemid,pHdr->subid);
     
    +    // find hot id first, luoyiming 2020-05-21
    +    if( (flag & NVOCMP_FINDLMASK) == NVOCMP_FINDSTRICT )
    +    {
    +      NVOCMP_hotItem_t hotItem = {.subid = pHdr->subid, .itemid = pHdr->itemid, .sysid = pHdr->sysid};
    +      hotItem.cmpid = cid;
    +      NVOCMP_hotNv_t* pHotNv = NVOCMP_hotItemMatch(hotItem);
    +      if( pHotNv )
    +      {
    +        NVOCMP_itemHdr_t iHdr;
    +        NVOCMP_readHeader(pHotNv->pg, pHotNv->ofs, &iHdr, false);
    +        if((iHdr.stats & NVOCMP_ACTIVEIDBIT) &&
    +          !(iHdr.stats & NVOCMP_VALIDIDBIT))
    +        {
    +          if( iHdr.cmpid == cid )
    +          {
    +            memcpy(pHdr, &iHdr, sizeof(NVOCMP_itemHdr_t));
    +            return(NVINTF_SUCCESS);
    +          }
    +        }
    +      }
    +    }
    +    else if((pInfo) && ((flag & NVOCMP_FINDHMASK) == NVOCMP_FINDCONTENT))
    +    {
    +      if( pHdr->subid == 0 )
    +      {
    +        NVOCMP_itemHdr_t iHdr;
    +        if(true == NVOCMP_hotItemMatchCont(pHdr->sysid, pHdr->itemid, pInfo, &iHdr))
    +        {
    +          if(!NVOCMP_readItem(&iHdr, 0, pInfo->rlength, pInfo->rBuf, false))
    +          {
    +            if(!memcmp((uint8_t *)pInfo->rBuf + pInfo->coff, pInfo->cBuf, pInfo->clength))
    +            {
    +              memcpy(pHdr, &iHdr, sizeof(NVOCMP_itemHdr_t));
    +              return(NVINTF_SUCCESS);
    +            }
    +          }
    +        }
    +      }
    +    }
    +
     #if (NVOCMP_NVPAGES > NVOCMP_NVTWOP)
         uint16_t nvSearched = 0;
         for(p = pg; nvSearched < NVOCMP_NVSIZE; p = NVOCMP_DECPAGE(p), ofs = pNvHandle->pageInfo[p].offset)
    @@ -3833,6 +3983,9 @@ static int8_t NVOCMP_findItem(NVOCMP_nvHandle_t *pNvHandle, uint8_t pg, uint16_t
                       if (cid == iHdr.cmpid)
                       {
                           found = true;
    +                      NVOCMP_hotItem_t hotItem = {.subid = iHdr.subid, .itemid = iHdr.itemid, .sysid = iHdr.sysid};
    +                      hotItem.cmpid = iHdr.cmpid;
    +                      NVOCMP_hotItemUpdate(p, ofs, hotItem);
                       }
                       break;
                   case NVOCMP_FINDSYSID:
    @@ -3862,8 +4015,14 @@ static int8_t NVOCMP_findItem(NVOCMP_nvHandle_t *pNvHandle, uint8_t pg, uint16_t
                     {
                       if(!NVOCMP_readItem(&iHdr, 0, pInfo->rlength, pInfo->rBuf, false))
                       {
    +                    // update hot item when read item success.
    +                    NVOCMP_hotItem_t hotItem = {.subid = iHdr.subid, .itemid = iHdr.itemid, .sysid = iHdr.sysid};
    +                    hotItem.cmpid = iHdr.cmpid;
    +                    NVOCMP_hotItemUpdate(p, ofs, hotItem);
    +
                         if(!memcmp((uint8_t *)pInfo->rBuf + pInfo->coff, pInfo->cBuf, pInfo->clength))
                         {
    +                      NVOCMP_hotItemUpdateCont(hotItem, pInfo->cBuf, pInfo->clength, pInfo->coff);
                           memcpy(pHdr, &iHdr, sizeof(NVOCMP_itemHdr_t));
                           return(NVINTF_SUCCESS);
                         }
    @@ -5028,6 +5187,119 @@ static uint8_t NVOCMP_verifyCRC(uint16_t iOfs, uint16_t len, uint8_t crc, uint8_
         return(newCRC == crc ? NVINTF_SUCCESS : NVINTF_CORRUPT);
     }
     
    +/*********************************************************************
    + * @fn      hotItemMatch
    + *
    + * @brief   Look for the parameter 'id' in the hot items array.
    + *
    + * @param   hotItem - A valid NV item.
    + *
    + * @return  A valid index into the hot items if the item is hot; OSAL_NV_MAX_HOT if not.
    + */
    +static NVOCMP_hotNv_t* NVOCMP_hotItemMatch(NVOCMP_hotItem_t hotItem)
    +{
    +  uint8_t nvNum = sizeof(NVOCMP_hotIdArray)/sizeof(NVOCMP_hotId_t);
    +  uint8_t n;
    +  for ( n=0; n<nvNum; n++ )
    +  {
    +    if( (hotItem.cmpid == NVOCMP_hotIdArray[n].cid) && (NVOCMP_hotIdArray[n].nv.vail == true) )
    +    {
    +      return &NVOCMP_hotIdArray[n].nv;
    +    }
    +  }
    +
    +  if( pfn_nvocmp_hotItemMatch )
    +  {
    +    return pfn_nvocmp_hotItemMatch(hotItem);
    +  }
    +  return NULL;
    +}
    +
    +/*********************************************************************
    + * @fn      hotItemUpdate
    + *
    + * @brief   If the parameter 'id' is a hot item, update the corresponding hot item data.
    + *
    + * @param   pg - The new NV page corresponding to the hot item.
    + * @param   off - The new NV page offset corresponding to the hot item.
    + * @param   hotItem - A valid NV item.
    + *
    + * @return  none
    + */
    +static void NVOCMP_hotItemUpdate(uint8_t pg, uint16_t ofs, NVOCMP_hotItem_t hotItem)
    +{
    +  uint8_t nvNum = sizeof(NVOCMP_hotIdArray)/sizeof(NVOCMP_hotId_t);
    +  uint8_t n;
    +  for ( n=0; n<nvNum; n++ )
    +  {
    +    if( hotItem.cmpid == NVOCMP_hotIdArray[n].cid )
    +    {
    +      NVOCMP_hotIdArray[n].nv.pg = pg;
    +      NVOCMP_hotIdArray[n].nv.ofs = ofs;
    +      NVOCMP_hotIdArray[n].nv.vail = true;
    +      return;
    +    }
    +  }
    +
    +  if( pfn_nvocmp_hotItemUpdate )
    +  {
    +    pfn_nvocmp_hotItemUpdate(pg, ofs, hotItem);
    +  }
    +}
    +
    +/*********************************************************************
    + * @fn      NVOCMP_hotItemMatchCont
    + *
    + * @brief   lookup NV in hot item when comparing content.
    + *
    + * @param   sysid - The sysid of item.
    + * @param   itemid - The itemid of hot item.
    + * @param   pInfo - pointer to item info.
    + * @param   pHdr - pointer to item header
    + *
    + * @return  none
    + */
    +static bool NVOCMP_hotItemMatchCont(uint8_t sysid, uint16_t itemid, NVOCMP_itemInfo_t *pInfo, NVOCMP_itemHdr_t* pHdr)
    +{
    +  NVOCMP_hotNv_t* hotNv = NULL;
    +  if( pfn_nvocmp_hotItemMatchCont )
    +  {
    +    hotNv = pfn_nvocmp_hotItemMatchCont(sysid, itemid, pInfo->cBuf, pInfo->clength, pInfo->coff);
    +    if( hotNv )
    +    {
    +      NVOCMP_readHeader(hotNv->pg, hotNv->ofs, pHdr, false);
    +      if((pHdr->stats & NVOCMP_ACTIVEIDBIT) && !(pHdr->stats & NVOCMP_VALIDIDBIT))
    +      {
    +        if((pHdr->sysid == sysid) && (pHdr->itemid == itemid))
    +        {
    +          return true;
    +        }
    +      }
    +    }
    +  }
    +  return false;
    +}
    +
    +/*********************************************************************
    + * @fn      NVOCMP_hotItemUpdateCont
    + *
    + * @brief   Update hot item that it can be lookup faster when comparing content.
    + *
    + * @param   hotItem - The hot item.
    + * @param   cBuf - pointer to caller's read data buffer
    + * @param   clen - length of NV data to return
    + * @param   coff - offset of content in data
    + *
    + * @return  none
    + */
    +static void NVOCMP_hotItemUpdateCont(NVOCMP_hotItem_t hotItem, void *cBuf, uint16_t clength, uint16_t coff)
    +{
    +  if( pfn_nvocmp_hotItemUpdateCont )
    +  {
    +    pfn_nvocmp_hotItemUpdateCont(hotItem, cBuf, clength, coff);
    +  }
    +}
    +
     #ifdef ENABLE_SANITY_CHECK
     /******************************************************************************
      * @fn      NVOCMP_sanityCheckApi
    @@ -5054,7 +5326,16 @@ static uint32_t NVOCMP_sanityCheckApi (void)
         uint8_t srcPg;
         uint32_t ret = NVINTF_SUCCESS;
         uint32_t aItem=0;
    +#ifdef NVOCMP_GPRAM
    +    uint32_t vm;
    +    uint8_t *pTBuffer = RAM_BUFFER_ADDRESS;
    +#else
    +    uint8_t *pTBuffer = (uint8_t *)tBuffer;
    +#endif
     
    +#ifndef NVOCMP_GPRAM
    +    memset(tBuffer, 0, sizeof(tBuffer));
    +#endif
         // Reset Flash erase/write fail indicator
         NVOCMP_failW = NVINTF_SUCCESS;
     
    @@ -5075,6 +5356,9 @@ static uint32_t NVOCMP_sanityCheckApi (void)
     
         NVOCMP_ALERT(false, "Sanity Check")
     
    +#ifdef NVOCMP_GPRAM
    +    NVOCMP_disableCache(&vm);
    +#endif
         while(srcOff > endOff)
         {
             if(NVOCMP_failW == NVINTF_SUCCESS)
    @@ -5144,6 +5428,12 @@ static uint32_t NVOCMP_sanityCheckApi (void)
                 {
                   if(!needSkip)
                   {
    +                // Get block of bytes from source page
    +#if NVOCMP_COMPR
    +                NVOCMP_read(srcPg, crcOff, (uint8_t *)(pTBuffer + dstOff), itemSize);
    +#else
    +                NVOCMP_read(srcPg, crcOff, (uint8_t *)(pTBuffer + FLASH_PAGE_SIZE - dstOff - itemSize), itemSize);
    +#endif
                     dstOff += itemSize;
                     aItem++;
                   }
    @@ -5153,6 +5443,9 @@ static uint32_t NVOCMP_sanityCheckApi (void)
             }
             else
             {
    +#ifdef NVOCMP_GPRAM
    +            NVOCMP_restoreCache(vm);
    +#endif
                 // Failure during item xfer makes next findItem() unreliable
                 NVOCMP_ASSERT(false, "SANITY CHECK FAILURE")
                 ret |= (1 << NVINTF_FAILURE);
    @@ -5161,11 +5454,18 @@ static uint32_t NVOCMP_sanityCheckApi (void)
     
         if(NVOCMP_failW != NVINTF_SUCCESS)
         {
    +#ifdef NVOCMP_GPRAM
    +        NVOCMP_restoreCache(vm);
    +#endif
             // Something bad happened when scanning the page
             NVOCMP_ASSERT(false, "SANITY CHECK FAILURE")
             ret |= (1 << NVINTF_FAILURE);
         }
     
    +#ifdef NVOCMP_GPRAM
    +    NVOCMP_restoreCache(vm);
    +#endif
    +
         return(ret);
     }
     #endif

    If anyone has made an attempt at the second part (TCLK table memory cache) I welcome your contribution.

  • I have researched Silabs's designing idea. The trust-center never store Joiner's APS-Key in its NV-RAM. The trust center will calculate joiner's APS-key from joiner's IEEE-address and trust-center's APS-Key-seed when the trust-center needs joiner's APS-key. The trust center only store joiner's install code in NV and delete it after joiner has joined.

  • That would be pretty awesome, although I'm guessing the APS key would also require a ZC known secret in its generation.

    Otherwise traffic would be reversable just from the IEEE addr which is not necessarily a secure secret.

    If you prototype that I'd be interested in seeing it.