Part Number: CC2652R7
Other Parts Discussed in Thread: SYSCONFIG
Question:
How do I instruct the lock-app build process to start the .nvs linker section at address 0xa8000 instead? The default value of 0xaa000 works fine for the 0x4000 bytes of internal NV defined for the lock-app (chip.syscfg) but in my case I’m defining an additional 0x2000 region that starts at address 0xa8000. This results in a total .nvs linker section of size 0x6000 instead of the default 0x4000 and yet the link step insists on starting the .nvs section at the default 0xaa000 instead of the 0xa8000. The result is that I get the following build failure.
FAILED: chip-LP_CC2652R7-lock-example.out chip-LP_CC2652R7-lock-example.out.map …. address 0xb0000 of ./chip-LP_CC2652R7-lock-example.out section `.nvs' is not within region `FLASH'
Details:
The following ‘grep’ command shows that something in the build system attempted to start the .nvs section starting at address 0xaa000. The 0x6000 bytes won’t fit if started there.
$ cd ~/TI/matter/examples/lock-app/cc13x2x7_26x2x7
$ grep "\.nvs" out/debug/chip-LP_CC2652R7-lock-example.out.map
.rodata.nvsCC26XXHWAttrs
.rodata.nvsSPI25XHWAttrs
.nvs 0x00000000000aa000 0x6000
*(.nvs)
.nvs 0x00000000000aa000 0x6000 obj/BUILD_DIR/gen/sysconfig/sysconfig.ti_drivers_config.c.o
.bss.nvsCC26XXObjects
.bss.nvsSPI25XObjects
The .nvs section needs to instead start at address 0xa8000 which is exactly the address that I indicated within chipsys.cfg for the additional nv region I defined.
Here are how the two regions are defined in my chip.syscfg
$ cd ~/TI/matter/examples/lock-app/cc13x2x7_26x2x7
$ grep "NVS1.internal" chip.syscfg
NVS1.internalFlash.$name = "ti_drivers_nvs_NVSCC26XX0";
NVS1.internalFlash.regionBase = 0xA8000;
NVS1.internalFlash.regionSize = 0x2000;
$ grep "NVS2.internal" chip.syscfg
NVS2.internalFlash.$name = "ti_drivers_nvs_NVSCC26XX1";
NVS2.internalFlash.regionBase = 0xAA000;
NVS2.internalFlash.regionSize = 0x4000;
Summary:
Since I have 0x6000 bytes of internal flash defined in chip.syscfg, and the starting address for the collection is 0xa8000, I will expect the lock-app build process to define the .nvs linker section to start at 0xa8000 (and not continue to use the default value of 0xaa000). Any ideas?