Part Number: CC2592EMK-RD
Other Parts Discussed in Thread: CC2592, CC2520
Hello
I have two questions about CC2592 application.
1. My project needs to use CC2520+CC2592. When I refer to the reference design of CC2538-CC2592EM and CC2592EM, I find that
the transmission lines from CC2592 output pin seem not to be 50 ohm. I wonder why the transmission lines are not 50 ohm.
2. My project will use a 6 layers stack-up. The prepreg thickness between layer1 and layer2 will be different with the reference design.
How should I design the impedance of transmission line from CC2592 output pin to antenna?
Thanks.