The commands section in ZAP Tool under the TI Matter repo does not display the Commands. For example. the Color Control Cluster has 19 commands, but none are shown:

Similar for the Level Control Cluster:

The "featurelevel" in the .zap is "81".
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The commands section in ZAP Tool under the TI Matter repo does not display the Commands. For example. the Color Control Cluster has 19 commands, but none are shown:

Similar for the Level Control Cluster:

The "featurelevel" in the .zap is "81".
Hi Joe,
Since TI does not independently maintain the *.zap files or develop the zap tool, I recommend that you download the latest zap tool from Github and modify your zap files from that repository. I am not seeing the same issue with featurelevel 94.
Regards,
Ryan