Part Number: CC1352P
Hello, there was such a problem: there is a СС1352P-4 with the installed firmware from the TI tempsensor openthread examples. There is also a border router with the latest software version from the open-thread repository. СС1352P-4 enters the network, everything works, but after 1-2 days the device disconnects from the network itself. I see only this in the logs:
May 26 02:57:59 ubuntu otbr-agent[1473]: 1d.03:44:53.134 [I] Mle-----------: Child timeout expired
May 26 02:57:59 ubuntu otbr-agent[1473]: 1d.03:44:53.135 [I] Settings------: Read ChildInfo {rloc:0x8001, extaddr:7a49fa192c4b2157, timeout:240, mode:0x0d, version:3}
May 26 02:57:59 ubuntu otbr-agent[1473]: 1d.03:44:53.143 [I] Settings------: Removed ChildInfo {rloc:0x8001, extaddr:7a49fa192c4b2157, timeout:240, mode:0x0d, version:3}
May 26 02:57:59 ubuntu otbr-agent[1473]: 1d.03:44:53.144 [I] Notifier------: StateChanged (0x00000800) [Child-]
May 26 02:57:59 ubuntu otbr-agent[1473]: 1d.03:44:53.144 [I] ChildSupervsn-: Stopping Child Supervision
May 26 17:19:36 ubuntu otbr-agent[1473]: 1d.18:06:30.879 [I] Mle-----------: Receive Child Update Request from child (fe80:0:0:0:7849:fa19:2c4b:2157)
May 26 17:19:36 ubuntu otbr-agent[1473]: 1d.18:06:30.879 [I] Mle-----------: Send Child Update Response to child (fe80:0:0:0:7849:fa19:2c4b:2157)
. Maybe there are some suggestions that this can be done?