Part Number: CC2652R
Other Parts Discussed in Thread: SIMPLELINK-CC13XX-CC26XX-SDK
Hi, I've got an application running on a CC2652R and somehow the on-board flash is very intermittently getting corrupted. Out of a sample size of around 50 prototype units running 24/7 for several months, we've seen the flash getting corrupted 3 times on different units. In our application, this corruption is essentially bricking our device.
Our application is directly calling the NV functions in the ZCL porting layer and its function pointers are set to use the NVOCMP driver functions in nvocmp.c. The call in my code that is failing is zclport_initializeNVItem(). I've traced down into this call in the debugger and it's failing at NVOCMP_findItem(), which is returning a value of NVINTF_CORRUPT.
Our application is currently using a total of 16 different NV items. When this corruption occurs, all of our items are reporting NVINTF_CORRUPT. The application basically writes to most of the NV items once at initialization and after that only reads those items at boot time. There is one NV item that is written to relatively frequently.
Two units ended up corrupted after writing their initialization values and came up bricked on the next boot. The other unit that ended up corrupted had been running a test that wrote to one specific item once every 15 minutes. In an attempt to reproduce the flash corruption, I set up another test unit to write to the same specific NV item continuously and it wrote thousands of times. So far, I have not been able to reproduce the problem.
To be clear, I'm only assuming that the most likely time that flash memory would get corrupted is during a write operation. I don't have any direct evidence that the corruption is occurring on a write operation.
Anyway, I'm trying to understand what could lead to this kind of corruption. What could lead to the NVOCMP functions returning NVINTF_CORRUPT?
While I wouldn't normally suspect a hardware component to this issue, it's interesting to note that we have another CC2652R based design that we have been testing for a considerably longer time and I have never seen the corruption on the other design. I haven't got enough of units to be statistically significant though.
Thanks,
Grant